Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.ALL_POINTS
All points use arclength
|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.FIRST_AND_SECOND_POINT
Only first and second point use arclength
|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.FIRST_AND_THIRD_POINT
Only first and third point use arclength
|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.FIRST_POINT
Only first point uses arclength
|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.NO_POINT
All points use percentage of arclength
|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.SECOND_AND_THIRD_POINT
Only second and third point use arclength
|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.SECOND_POINT
Only second point uses arclength
|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.THIRD_POINT
Only third point uses arclength
|
Modifier and Type | Method and Description |
---|---|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumPlaneBuilder.UseArcLength |
DatumPlaneBuilder.UseArcLength.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumPlaneBuilder.UseArcLength[] |
DatumPlaneBuilder.UseArcLength.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumPlaneBuilder.setThreePoints(Point point1,
Point point2,
Point point3,
DatumPlaneBuilder.UseArcLength useArcLength)
Sets three different points.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.