Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.BINORMAL
Datum plane at binormal to curve
|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.NORMAL
Datum plane at normal to curve
|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.OPPOSITE_BINORMAL
Datum plane at opposite to binormal to curve
|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.OPPOSITE_NORMAL
Datum plane at opposite to normal to curve
|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.OPPOSITE_TANGENT
Datum plane at opposite to tangent to curve
|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.PROJECT
This direction is calculated by projecting a point selected along a curve
to a line, a datum axis, an edge of a solid, a planar face or a datum plane
|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.PROJECT_VIEW
Datum plane direction is calculated during creation based on the view plane.
|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.TANGENT
Indicates the datum plane as tangent to curve
|
Modifier and Type | Method and Description |
---|---|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumPlaneBuilder.AlternateSolution |
DatumPlaneBuilder.AlternateSolution.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumPlaneBuilder.AlternateSolution[] |
DatumPlaneBuilder.AlternateSolution.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumPlaneBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumPlaneBuilder.AlternateSolution alternateSolution,
DatumPlaneBuilder.CurveOption option,
ICurve curve)
Sets curve or edge and arc length
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
void |
DatumPlaneBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumPlaneBuilder.AlternateSolution alternateSolution,
DatumPlaneBuilder.CurveOption option,
ICurve curve,
nxopen.Direction direction)
Sets curve or edge and arc length
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.