Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumAxisBuilder.UseArcLength |
DatumAxisBuilder.UseArcLength.ALL_POINTS
Both points use arclength
|
static DatumAxisBuilder.UseArcLength |
DatumAxisBuilder.UseArcLength.FIRST_POINT
Only first point uses arclength
|
static DatumAxisBuilder.UseArcLength |
DatumAxisBuilder.UseArcLength.NO_POINT
All points use percentage of arclength
|
static DatumAxisBuilder.UseArcLength |
DatumAxisBuilder.UseArcLength.SECOND_POINT
Only second point uses arclength
|
Modifier and Type | Method and Description |
---|---|
static DatumAxisBuilder.UseArcLength |
DatumAxisBuilder.UseArcLength.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumAxisBuilder.UseArcLength |
DatumAxisBuilder.UseArcLength.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumAxisBuilder.UseArcLength[] |
DatumAxisBuilder.UseArcLength.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumAxisBuilder.setTwoPoints(Point point1,
Point point2,
DatumAxisBuilder.UseArcLength useArcLength)
Sets two points
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.