Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumAxisBuilder.CurveOption |
DatumAxisBuilder.CurveOption.DISTANCE
Absolute distance
|
static DatumAxisBuilder.CurveOption |
DatumAxisBuilder.CurveOption.PERCENT
Relative distance as percentage
|
Modifier and Type | Method and Description |
---|---|
static DatumAxisBuilder.CurveOption |
DatumAxisBuilder.CurveOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumAxisBuilder.CurveOption |
DatumAxisBuilder.CurveOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumAxisBuilder.CurveOption[] |
DatumAxisBuilder.CurveOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumAxisBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumAxisBuilder.AlternateSolution alternateSolution,
DatumAxisBuilder.CurveOption option,
ICurve curve)
Sets curve or edge and arc length
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
DatumAxisBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumAxisBuilder.CurveOption option,
DisplayableObject secondGeometry,
ICurve curve)
Sets Curve or Edge object and arc length with an extra geometry in picture
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
DatumAxisBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumAxisBuilder.CurveOption option,
ICurve curve,
DisplayableObject secondGeometry)
Sets Curve or Edge object and arc length with an extra geometry in picture
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.