Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static CopyPasteBuilder.ParentSelectOption |
CopyPasteBuilder.ParentSelectOption.INPUT_FOR_ORIGINAL_PARENT
Specifying smart object using the same creation method that was used in the original feature.
|
static CopyPasteBuilder.ParentSelectOption |
CopyPasteBuilder.ParentSelectOption.SMART_OBJECT
Selecting input for the original parent.
|
Modifier and Type | Method and Description |
---|---|
CopyPasteBuilder.ParentSelectOption |
CopyPasteBuilder.selectOption()
Returns the parent select option.
|
static CopyPasteBuilder.ParentSelectOption |
CopyPasteBuilder.ParentSelectOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CopyPasteBuilder.ParentSelectOption |
CopyPasteBuilder.ParentSelectOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CopyPasteBuilder.ParentSelectOption[] |
CopyPasteBuilder.ParentSelectOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CopyPasteBuilder.setSelectOption(CopyPasteBuilder.ParentSelectOption selectionOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.