Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static CompositeCurveBuilder.PartType |
CompositeCurveBuilder.PartType.OTHER_PART
Other part in assembly
|
static CompositeCurveBuilder.PartType |
CompositeCurveBuilder.PartType.WORK_PART
Work part
|
Modifier and Type | Method and Description |
---|---|
CompositeCurveBuilder.PartType |
CompositeCurveBuilder.parentPart()
Returns the parent part
License requirements: None. |
static CompositeCurveBuilder.PartType |
CompositeCurveBuilder.PartType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CompositeCurveBuilder.PartType |
CompositeCurveBuilder.PartType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CompositeCurveBuilder.PartType[] |
CompositeCurveBuilder.PartType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CompositeCurveBuilder.setParentPart(CompositeCurveBuilder.PartType parentPart)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.