Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static CircularBlendCurveBuilder.CylinderRadiusOption |
CircularBlendCurveBuilder.CylinderRadiusOption.POINT_ON_FIRST_CURVE
Radius by point on first curve
|
static CircularBlendCurveBuilder.CylinderRadiusOption |
CircularBlendCurveBuilder.CylinderRadiusOption.POINT_ON_SECOND_CURVE
Radius by point on second curve
|
static CircularBlendCurveBuilder.CylinderRadiusOption |
CircularBlendCurveBuilder.CylinderRadiusOption.VALUE
Radius by value
|
Modifier and Type | Method and Description |
---|---|
CircularBlendCurveBuilder.CylinderRadiusOption |
CircularBlendCurveBuilder.radiusOption()
Returns the cylinder radius option as
CircularBlendCurveBuilder.CylinderRadiusOption
License requirements: None. |
static CircularBlendCurveBuilder.CylinderRadiusOption |
CircularBlendCurveBuilder.CylinderRadiusOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CircularBlendCurveBuilder.CylinderRadiusOption |
CircularBlendCurveBuilder.CylinderRadiusOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CircularBlendCurveBuilder.CylinderRadiusOption[] |
CircularBlendCurveBuilder.CylinderRadiusOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CircularBlendCurveBuilder.setRadiusOption(CircularBlendCurveBuilder.CylinderRadiusOption radiusOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.