Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilderEx.ShapeControlMethods |
BridgeCurveBuilderEx.ShapeControlMethods.CONIC
Shape using rho value of a conic.
|
static BridgeCurveBuilderEx.ShapeControlMethods |
BridgeCurveBuilderEx.ShapeControlMethods.DEPTH_SKEW
Shape using depth and skew value
|
static BridgeCurveBuilderEx.ShapeControlMethods |
BridgeCurveBuilderEx.ShapeControlMethods.TANGENT_MAGNITUDE
Shape using tangent magnitude at ends
|
static BridgeCurveBuilderEx.ShapeControlMethods |
BridgeCurveBuilderEx.ShapeControlMethods.TEMPLATE_CURVE
Shape by a template curve
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilderEx.ShapeControlMethods |
BridgeCurveBuilderEx.shapeControlMethod()
Returns the shape control method
License requirements: None. |
static BridgeCurveBuilderEx.ShapeControlMethods |
BridgeCurveBuilderEx.ShapeControlMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilderEx.ShapeControlMethods |
BridgeCurveBuilderEx.ShapeControlMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilderEx.ShapeControlMethods[] |
BridgeCurveBuilderEx.ShapeControlMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilderEx.setShapeControlMethod(BridgeCurveBuilderEx.ShapeControlMethods shapeControlMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.