Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilder.EndObjectTypes |
BridgeCurveBuilder.EndObjectTypes.OBJECT
allowed end object type except a vector object
|
static BridgeCurveBuilder.EndObjectTypes |
BridgeCurveBuilder.EndObjectTypes.VECTOR
vector object
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilder.EndObjectTypes |
BridgeCurveBuilder.endObjectOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
static BridgeCurveBuilder.EndObjectTypes |
BridgeCurveBuilder.EndObjectTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.EndObjectTypes |
BridgeCurveBuilder.EndObjectTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.EndObjectTypes[] |
BridgeCurveBuilder.EndObjectTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilder.setEndObjectOption(BridgeCurveBuilder.EndObjectTypes endObjectOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.