Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilder.CurveFitTypes |
BridgeCurveBuilder.CurveFitTypes.ADVANCED
general fit curve
|
static BridgeCurveBuilder.CurveFitTypes |
BridgeCurveBuilder.CurveFitTypes.CUBIC
fit curve with 3 degrees
|
static BridgeCurveBuilder.CurveFitTypes |
BridgeCurveBuilder.CurveFitTypes.QUINTIC
fit curve with 5 degrees
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilder.CurveFitTypes |
BridgeCurveBuilder.curveFitOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
static BridgeCurveBuilder.CurveFitTypes |
BridgeCurveBuilder.CurveFitTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.CurveFitTypes |
BridgeCurveBuilder.CurveFitTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.CurveFitTypes[] |
BridgeCurveBuilder.CurveFitTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilder.setCurveFitOption(BridgeCurveBuilder.CurveFitTypes curveFitOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.