Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AssociativeArcBuilder.Types |
AssociativeArcBuilder.Types.ARC_FROM_CENTER
Arc from center
|
static AssociativeArcBuilder.Types |
AssociativeArcBuilder.Types.THREE_POINT_ARC
Three point arc
|
Modifier and Type | Method and Description |
---|---|
AssociativeArcBuilder.Types |
AssociativeArcBuilder.type()
Returns the type option
License requirements: None. |
static AssociativeArcBuilder.Types |
AssociativeArcBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativeArcBuilder.Types |
AssociativeArcBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativeArcBuilder.Types[] |
AssociativeArcBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssociativeArcBuilder.setType(AssociativeArcBuilder.Types type)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.