Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AssociativeArcBuilder.StartOption |
AssociativeArcBuilder.StartOption.INFERRED
Inferred
|
static AssociativeArcBuilder.StartOption |
AssociativeArcBuilder.StartOption.POINT
Point
|
static AssociativeArcBuilder.StartOption |
AssociativeArcBuilder.StartOption.TANGENT
Tangent
|
Modifier and Type | Method and Description |
---|---|
AssociativeArcBuilder.StartOption |
AssociativeArcBuilder.startPointOptions()
Returns the start point options
License requirements: None. |
static AssociativeArcBuilder.StartOption |
AssociativeArcBuilder.StartOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativeArcBuilder.StartOption |
AssociativeArcBuilder.StartOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativeArcBuilder.StartOption[] |
AssociativeArcBuilder.StartOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssociativeArcBuilder.setStartPointOptions(AssociativeArcBuilder.StartOption startPointOptions)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.