Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AssociativeArcBuilder.MidOption |
AssociativeArcBuilder.MidOption.DIAMETER
Diameter
|
static AssociativeArcBuilder.MidOption |
AssociativeArcBuilder.MidOption.INFERRED
Inferred
|
static AssociativeArcBuilder.MidOption |
AssociativeArcBuilder.MidOption.POINT
Point
|
static AssociativeArcBuilder.MidOption |
AssociativeArcBuilder.MidOption.RADIUS
Radius
|
static AssociativeArcBuilder.MidOption |
AssociativeArcBuilder.MidOption.TANGENT
Tangent
|
Modifier and Type | Method and Description |
---|---|
AssociativeArcBuilder.MidOption |
AssociativeArcBuilder.midPointOptions()
Returns the mid point options
License requirements: None. |
static AssociativeArcBuilder.MidOption |
AssociativeArcBuilder.MidOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AssociativeArcBuilder.MidOption |
AssociativeArcBuilder.MidOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AssociativeArcBuilder.MidOption[] |
AssociativeArcBuilder.MidOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AssociativeArcBuilder.setMidPointOptions(AssociativeArcBuilder.MidOption midPointOptions)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.