Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AestheticFaceBlendBuilder.BlendType |
AestheticFaceBlendBuilder.BlendType.CHORD_LENGTH
Chord Length will keep the appearance of a constant width blend through areas which have changing angles between the input walls.
|
static AestheticFaceBlendBuilder.BlendType |
AestheticFaceBlendBuilder.BlendType.RADIUS
Radius of the rolling ball is used to create the tangent lines.
|
Modifier and Type | Method and Description |
---|---|
AestheticFaceBlendBuilder.BlendType |
AestheticFaceBlendBuilder.blendOption()
Returns the method option
License requirements: None. |
static AestheticFaceBlendBuilder.BlendType |
AestheticFaceBlendBuilder.BlendType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.BlendType |
AestheticFaceBlendBuilder.BlendType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.BlendType[] |
AestheticFaceBlendBuilder.BlendType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AestheticFaceBlendBuilder.setBlendOption(AestheticFaceBlendBuilder.BlendType blendOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.