Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AestheticFaceBlendBuilder.BlendFacesType |
AestheticFaceBlendBuilder.BlendFacesType.DO_NOT_TRIM_BLEND_FACES
This option controls to trim blend faces or not
|
static AestheticFaceBlendBuilder.BlendFacesType |
AestheticFaceBlendBuilder.BlendFacesType.TRIMTO_ALL_INPUT_FACES
Trims all input faces.
|
static AestheticFaceBlendBuilder.BlendFacesType |
AestheticFaceBlendBuilder.BlendFacesType.TRIMTO_LONG_INPUT_FACES
Trims long input faces.
|
static AestheticFaceBlendBuilder.BlendFacesType |
AestheticFaceBlendBuilder.BlendFacesType.TRIMTO_SHORT_INPUT_FACES
Trims short input faces.
|
Modifier and Type | Method and Description |
---|---|
AestheticFaceBlendBuilder.BlendFacesType |
AestheticFaceBlendBuilder.blendFacesOption()
Returns the blend faces option
License requirements: None. |
static AestheticFaceBlendBuilder.BlendFacesType |
AestheticFaceBlendBuilder.BlendFacesType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.BlendFacesType |
AestheticFaceBlendBuilder.BlendFacesType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.BlendFacesType[] |
AestheticFaceBlendBuilder.BlendFacesType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AestheticFaceBlendBuilder.setBlendFacesOption(AestheticFaceBlendBuilder.BlendFacesType blendFacesOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.