Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AOCSBuilder.OffsetDirection |
AOCSBuilder.OffsetDirection.NORMAL_TO_CURVE
traditional curve normal
|
static AOCSBuilder.OffsetDirection |
AOCSBuilder.OffsetDirection.NORMAL_TO_VECTOR
offset pependicular to vector
|
Modifier and Type | Method and Description |
---|---|
AOCSBuilder.OffsetDirection |
AOCSBuilder.offsetDirectionOption()
Returns the offset direction vector
License requirements: solid_modeling ("SOLIDS MODELING") . |
static AOCSBuilder.OffsetDirection |
AOCSBuilder.OffsetDirection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AOCSBuilder.OffsetDirection |
AOCSBuilder.OffsetDirection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AOCSBuilder.OffsetDirection[] |
AOCSBuilder.OffsetDirection.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AOCSBuilder.setOffsetDirectionOption(AOCSBuilder.OffsetDirection direction)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.