public interface ToolingCollection extends TaggedObjectCollection
FeatureCollection
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
PrebendBuilder |
createPrebendBuilder(Prebend prebend)
Creates a
PrebendBuilder
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") Created in NX10.0.0 |
UniversalUnformBuilder |
createUniversalUnformBuilder(UniversalUnform universalUnform)
Creates a
UniversalUnformBuilder
License requirements: prog_die_wizard ("UG/Progressive Die Wizard") Created in NX8.5.0 |
Feature |
toolingFindObject(String journalIdentifier)
Finds the
nxopen.features with the given identifier as
recorded in a journal. |
_find_next, iterator
UniversalUnformBuilder createUniversalUnformBuilder(UniversalUnform universalUnform) throws NXException, RemoteException
UniversalUnformBuilder
universalUnform
- UniversalUnform
to be editedNXException
RemoteException
PrebendBuilder createPrebendBuilder(Prebend prebend) throws NXException, RemoteException
PrebendBuilder
prebend
- Prebend
to be editedNXException
RemoteException
Feature toolingFindObject(String journalIdentifier) throws NXException, RemoteException
nxopen.features
with the given identifier as
recorded in a journal. An object may not return the same value as its JournalIdentifier
in different versions of the software. However newer versions of the software should find
the same object when FindObject is passed older versions of its journal identifier. In general,
this method should not be used in handwritten code and exists to support record and
playback of journals.
journalIdentifier
- Identifier to be foundNXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.