public static class StepBuilder.StepWallMethods extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXTENDTO_NEXT
Extends the wall face to intersect the next face
|
static int |
_NORMAL
Orients the step-wall face normal to the input face
|
static int |
_OFFSETOF_STEP_FACE
Makes the step-wall face offset from the step face
|
static StepBuilder.StepWallMethods |
EXTENDTO_NEXT
Extends the wall face to intersect the next face
|
static StepBuilder.StepWallMethods |
NORMAL
Orients the step-wall face normal to the input face
|
static StepBuilder.StepWallMethods |
OFFSETOF_STEP_FACE
Makes the step-wall face offset from the step face
|
Modifier and Type | Method and Description |
---|---|
static StepBuilder.StepWallMethods |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.StepWallMethods |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.StepWallMethods[] |
values()
Returns an array that contains the values for this enum.
|
public static final StepBuilder.StepWallMethods NORMAL
public static final StepBuilder.StepWallMethods OFFSETOF_STEP_FACE
public static final StepBuilder.StepWallMethods EXTENDTO_NEXT
public static final int _NORMAL
public static final int _OFFSETOF_STEP_FACE
public static final int _EXTENDTO_NEXT
public static StepBuilder.StepWallMethods valueOf(int value)
public static StepBuilder.StepWallMethods valueOf(String name)
public static StepBuilder.StepWallMethods[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.