public static class StepBuilder.StepTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CHAMFER
Adds a step at the edge of a face similar to a chamfer
|
static int |
_END
Adds a step from a boundary to the edge of a face.
|
static int |
_MIDDLE
Adds a step between two boundary curves
|
static StepBuilder.StepTypes |
CHAMFER
Adds a step at the edge of a face similar to a chamfer
|
static StepBuilder.StepTypes |
END
Adds a step from a boundary to the edge of a face.
|
static StepBuilder.StepTypes |
MIDDLE
Adds a step between two boundary curves
|
Modifier and Type | Method and Description |
---|---|
static StepBuilder.StepTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.StepTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.StepTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final StepBuilder.StepTypes END
public static final StepBuilder.StepTypes MIDDLE
public static final StepBuilder.StepTypes CHAMFER
public static final int _END
public static final int _MIDDLE
public static final int _CHAMFER
public static StepBuilder.StepTypes valueOf(int value)
public static StepBuilder.StepTypes valueOf(String name)
public static StepBuilder.StepTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.