public static class SectionSurfaceBuilderEx.SpineEndFlowType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ISO_LINE_U
flow direction follows iso u of the start surface
|
static int |
_ISO_LINE_V
flow direction follows iso v of the start surface
|
static int |
_NOT_SPECIFIED
flow direction not specified
|
static int |
_PERPENDICULAR
flow direction perpendicular to the guide
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
ISO_LINE_U
flow direction follows iso u of the start surface
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
ISO_LINE_V
flow direction follows iso v of the start surface
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
NOT_SPECIFIED
flow direction not specified
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
PERPENDICULAR
flow direction perpendicular to the guide
|
Modifier and Type | Method and Description |
---|---|
static SectionSurfaceBuilderEx.SpineEndFlowType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilderEx.SpineEndFlowType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilderEx.SpineEndFlowType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SectionSurfaceBuilderEx.SpineEndFlowType NOT_SPECIFIED
public static final SectionSurfaceBuilderEx.SpineEndFlowType PERPENDICULAR
public static final SectionSurfaceBuilderEx.SpineEndFlowType ISO_LINE_U
public static final SectionSurfaceBuilderEx.SpineEndFlowType ISO_LINE_V
public static final int _NOT_SPECIFIED
public static final int _PERPENDICULAR
public static final int _ISO_LINE_U
public static final int _ISO_LINE_V
public static SectionSurfaceBuilderEx.SpineEndFlowType valueOf(int value)
public static SectionSurfaceBuilderEx.SpineEndFlowType valueOf(String name)
public static SectionSurfaceBuilderEx.SpineEndFlowType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.