public interface ResizeCurveBuilder
ResizeCurve
builder
SynchronousCurveCollection.createResizeCurveBuilder(nxopen.features.ResizeCurve)
Property | Value |
---|---|
CurveFinder.ChamferEnabled | 0 |
CurveFinder.CoincidentVertexEnabled | 0 |
CurveFinder.CollinearEnabled | 0 |
CurveFinder.ConcentricEnabled | 0 |
CurveFinder.EqualRadiusEnabled | 0 |
CurveFinder.OffsetEnabled | 0 |
CurveFinder.ParallelEnabled | 0 |
CurveFinder.SymmetricEnabled | 0 |
CurveFinder.TangentEnabled | 0 |
CurveFinder.UseCurveFinder | 1 |
CurveFinder.VertexOnCurveEnabled | 0 |
ValueOption | Diameter |
Modifier and Type | Interface and Description |
---|---|
static class |
ResizeCurveBuilder.ValueType
the option for radius or diameter
|
Modifier and Type | Method and Description |
---|---|
CurveFinderBuilder |
curveFinder()
Returns the curve section
License requirements: None. |
double |
distanceTolerance()
Returns the distance tolerance
License requirements: None. |
boolean |
keepOrthogonal()
Returns a value that indicates whether keep orthogonal is enabled
License requirements: None. |
void |
setDistanceTolerance(double distanceTolerance)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setKeepOrthogonal(boolean keepOrthogonal)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setValueOption(ResizeCurveBuilder.ValueType valueOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Expression |
value()
Returns the value to resize
License requirements: None. |
ResizeCurveBuilder.ValueType |
valueOption()
Returns the size option
License requirements: None. |
CurveFinderBuilder curveFinder() throws NXException, RemoteException
NXException
RemoteException
Expression value() throws NXException, RemoteException
NXException
RemoteException
ResizeCurveBuilder.ValueType valueOption() throws NXException, RemoteException
NXException
RemoteException
void setValueOption(ResizeCurveBuilder.ValueType valueOption) throws NXException, RemoteException
valueOption
- NXException
RemoteException
double distanceTolerance() throws NXException, RemoteException
NXException
RemoteException
void setDistanceTolerance(double distanceTolerance) throws NXException, RemoteException
distanceTolerance
- NXException
RemoteException
boolean keepOrthogonal() throws NXException, RemoteException
NXException
RemoteException
void setKeepOrthogonal(boolean keepOrthogonal) throws NXException, RemoteException
keepOrthogonal
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.