public static class PasteFaceBuilder.PasteOptionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADD
each tool body will add to the target body.
|
static int |
_AUTOMATIC
determined automatically from the 'add' or 'subtract' attributes on each tool body.
|
static int |
_SUBTRACT
each tool body will subtract from the target body.
|
static PasteFaceBuilder.PasteOptionType |
ADD
each tool body will add to the target body.
|
static PasteFaceBuilder.PasteOptionType |
AUTOMATIC
determined automatically from the 'add' or 'subtract' attributes on each tool body.
|
static PasteFaceBuilder.PasteOptionType |
SUBTRACT
each tool body will subtract from the target body.
|
Modifier and Type | Method and Description |
---|---|
static PasteFaceBuilder.PasteOptionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PasteFaceBuilder.PasteOptionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PasteFaceBuilder.PasteOptionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PasteFaceBuilder.PasteOptionType AUTOMATIC
public static final PasteFaceBuilder.PasteOptionType ADD
public static final PasteFaceBuilder.PasteOptionType SUBTRACT
public static final int _AUTOMATIC
public static final int _ADD
public static final int _SUBTRACT
public static PasteFaceBuilder.PasteOptionType valueOf(int value)
public static PasteFaceBuilder.PasteOptionType valueOf(String name)
public static PasteFaceBuilder.PasteOptionType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.