public static class PartModule.PartLoadOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DONT_ALLOW_SAVE
Sets the loaded part as read only.
|
static int |
_LOAD_INTERPART
If this option is set, First it will check part is modified or not, then loads interpart of Part Module otherwise reload the own part of Part Module
|
static PartModule.PartLoadOption |
DONT_ALLOW_SAVE
Sets the loaded part as read only.
|
static PartModule.PartLoadOption |
LOAD_INTERPART
If this option is set, First it will check part is modified or not, then loads interpart of Part Module otherwise reload the own part of Part Module
|
Modifier and Type | Method and Description |
---|---|
static PartModule.PartLoadOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartModule.PartLoadOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartModule.PartLoadOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartModule.PartLoadOption DONT_ALLOW_SAVE
public static final PartModule.PartLoadOption LOAD_INTERPART
public static final int _DONT_ALLOW_SAVE
public static final int _LOAD_INTERPART
public static PartModule.PartLoadOption valueOf(int value)
public static PartModule.PartLoadOption valueOf(String name)
public static PartModule.PartLoadOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.