public static class PartGeometryCopyBuilder.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
An option to select point, datum, sketch, body, and curve feature
|
static int |
_BODY_COLLECTOR
An option to select bodies via body selection intent
|
static int |
_BODY_OBJECT
An option to select body, body-based feature, and body group
|
static int |
_COMPOSITE_CURVE
An option to composite a curve via curve selection intent
|
static int |
_COMPOSITE_FACE
An option to composite a body via face selection intent
|
static int |
_CURVE
Curve or edge
|
static int |
_CURVE_FEATURE
Curve-based feature
|
static int |
_DATUM
Datum plane, datum axis or datum coordinate system feature
|
static int |
_EXPRESSION
Expression
|
static int |
_FACE
Face
|
static int |
_PMI
PMI dimension
|
static int |
_POINT
Point
|
static int |
_ROUTING_OBJECT
Routing Object
|
static int |
_SKETCH
Sketch feature
|
static PartGeometryCopyBuilder.Type |
AUTOMATIC
An option to select point, datum, sketch, body, and curve feature
|
static PartGeometryCopyBuilder.Type |
BODY_COLLECTOR
An option to select bodies via body selection intent
|
static PartGeometryCopyBuilder.Type |
BODY_OBJECT
An option to select body, body-based feature, and body group
|
static PartGeometryCopyBuilder.Type |
COMPOSITE_CURVE
An option to composite a curve via curve selection intent
|
static PartGeometryCopyBuilder.Type |
COMPOSITE_FACE
An option to composite a body via face selection intent
|
static PartGeometryCopyBuilder.Type |
CURVE
Curve or edge
|
static PartGeometryCopyBuilder.Type |
CURVE_FEATURE
Curve-based feature
|
static PartGeometryCopyBuilder.Type |
DATUM
Datum plane, datum axis or datum coordinate system feature
|
static PartGeometryCopyBuilder.Type |
EXPRESSION
Expression
|
static PartGeometryCopyBuilder.Type |
FACE
Face
|
static PartGeometryCopyBuilder.Type |
PMI
PMI dimension
|
static PartGeometryCopyBuilder.Type |
POINT
Point
|
static PartGeometryCopyBuilder.Type |
ROUTING_OBJECT
Routing Object
|
static PartGeometryCopyBuilder.Type |
SKETCH
Sketch feature
|
Modifier and Type | Method and Description |
---|---|
static PartGeometryCopyBuilder.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartGeometryCopyBuilder.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartGeometryCopyBuilder.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartGeometryCopyBuilder.Type AUTOMATIC
public static final PartGeometryCopyBuilder.Type BODY_COLLECTOR
public static final PartGeometryCopyBuilder.Type BODY_OBJECT
public static final PartGeometryCopyBuilder.Type CURVE_FEATURE
public static final PartGeometryCopyBuilder.Type SKETCH
public static final PartGeometryCopyBuilder.Type DATUM
public static final PartGeometryCopyBuilder.Type POINT
public static final PartGeometryCopyBuilder.Type COMPOSITE_CURVE
public static final PartGeometryCopyBuilder.Type COMPOSITE_FACE
public static final PartGeometryCopyBuilder.Type EXPRESSION
public static final PartGeometryCopyBuilder.Type PMI
public static final PartGeometryCopyBuilder.Type CURVE
public static final PartGeometryCopyBuilder.Type FACE
public static final PartGeometryCopyBuilder.Type ROUTING_OBJECT
public static final int _AUTOMATIC
public static final int _BODY_COLLECTOR
public static final int _BODY_OBJECT
public static final int _CURVE_FEATURE
public static final int _SKETCH
public static final int _DATUM
public static final int _POINT
public static final int _COMPOSITE_CURVE
public static final int _COMPOSITE_FACE
public static final int _EXPRESSION
public static final int _PMI
public static final int _CURVE
public static final int _FACE
public static final int _ROUTING_OBJECT
public static PartGeometryCopyBuilder.Type valueOf(int value)
public static PartGeometryCopyBuilder.Type valueOf(String name)
public static PartGeometryCopyBuilder.Type[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.