public interface MoveEdgeBuilder
MoveEdge
builder
SynchronousEdgeCollection.createMoveEdgeBuilder(nxopen.features.MoveEdge)
Property | Value |
---|---|
Motion.DeltaEnum | ReferenceWcsWorkPart |
Motion.DeltaXc.Value | 0.0 |
Motion.DeltaYc.Value | 0.0 |
Motion.DeltaZc.Value | 0.0 |
Motion.Option | Distance |
Modifier and Type | Interface and Description |
---|---|
static class |
MoveEdgeBuilder.EndFaceBehaviorType
Represents the end face behavior.
|
Modifier and Type | Method and Description |
---|---|
ScCollector |
edgeToMove()
Returns the edge collector.
|
MoveEdgeBuilder.EndFaceBehaviorType |
endFaceBehavior()
Returns the end face setting.
|
ModlMotion |
motion()
Returns the motion which record the move behaviour.
|
void |
setEndFaceBehavior(MoveEdgeBuilder.EndFaceBehaviorType type)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
ScCollector edgeToMove() throws NXException, RemoteException
NXException
RemoteException
ModlMotion motion() throws NXException, RemoteException
NXException
RemoteException
MoveEdgeBuilder.EndFaceBehaviorType endFaceBehavior() throws NXException, RemoteException
NXException
RemoteException
void setEndFaceBehavior(MoveEdgeBuilder.EndFaceBehaviorType type) throws NXException, RemoteException
type
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.