public interface MoveCurveBuilder
MoveCurve
builder
SynchronousCurveCollection.createMoveCurveBuilder(nxopen.features.MoveCurve)
Property | Value |
---|---|
CurveFinder.ChamferEnabled | 0 |
CurveFinder.CoincidentVertexEnabled | 0 |
CurveFinder.CollinearEnabled | 0 |
CurveFinder.ConcentricEnabled | 0 |
CurveFinder.EqualRadiusEnabled | 0 |
CurveFinder.OffsetEnabled | 0 |
CurveFinder.ParallelEnabled | 0 |
CurveFinder.SymmetricEnabled | 0 |
CurveFinder.TangentEnabled | 0 |
CurveFinder.UseCurveFinder | 1 |
CurveFinder.VertexOnCurveEnabled | 0 |
TransformMotion.DeltaEnum | ReferenceWcsWorkPart |
TransformMotion.DeltaXc.Value | 0.0 |
TransformMotion.DeltaYc.Value | 0.0 |
TransformMotion.DeltaZc.Value | 0.0 |
TransformMotion.Option | Dynamic |
Modifier and Type | Method and Description |
---|---|
CurveFinderBuilder |
curveFinder()
Returns the curve section
License requirements: None. |
double |
distanceTolerance()
Returns the distance tolerance
License requirements: None. |
boolean |
keepOrthogonal()
Returns a value that indicates whether keep orthogonal is enabled
License requirements: None. |
int |
keepTangent()
Returns a value that indicates which keep tangent support is selected
License requirements: None. |
void |
setDistanceTolerance(double distanceTolerance)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
setKeepOrthogonal(boolean keepOrthogonal)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
setKeepTangent(int keepTangent)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
setSizeOption(int sizeOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
int |
sizeOption()
Returns a value that indicates which size option is selected
License requirements: None. |
ModlMotion |
transformMotion()
Returns the transform motion
License requirements: None. |
CurveFinderBuilder curveFinder() throws NXException, RemoteException
NXException
RemoteException
ModlMotion transformMotion() throws NXException, RemoteException
NXException
RemoteException
double distanceTolerance() throws NXException, RemoteException
NXException
RemoteException
void setDistanceTolerance(double distanceTolerance) throws NXException, RemoteException
distanceTolerance
- NXException
RemoteException
int sizeOption() throws NXException, RemoteException
NXException
RemoteException
void setSizeOption(int sizeOption) throws NXException, RemoteException
sizeOption
- NXException
RemoteException
int keepTangent() throws NXException, RemoteException
NXException
RemoteException
void setKeepTangent(int keepTangent) throws NXException, RemoteException
keepTangent
- NXException
RemoteException
boolean keepOrthogonal() throws NXException, RemoteException
NXException
RemoteException
void setKeepOrthogonal(boolean keepOrthogonal) throws NXException, RemoteException
keepOrthogonal
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.