public static class MatchedReferenceBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AXIS
axis
|
static int |
_BODY_COLLECTOR
body collector
|
static int |
_CSYS
csys
|
static int |
_CURVE
single curve or edge
|
static int |
_CURVE_COLLECTOR
curve collector or edge collector
|
static int |
_FACE
single face or datum plane
|
static int |
_FACE_COLLECTOR
face collector
|
static int |
_OBJECT
general geometry such as the target body and the tool body for copying unite feature
|
static int |
_PLANE
plane
|
static int |
_POINT
point
|
static int |
_SECTION
section
|
static int |
_UNDEFINED
default type for feature name lable
|
static int |
_VECTOR
vector
|
static MatchedReferenceBuilder.Types |
AXIS
axis
|
static MatchedReferenceBuilder.Types |
BODY_COLLECTOR
body collector
|
static MatchedReferenceBuilder.Types |
CSYS
csys
|
static MatchedReferenceBuilder.Types |
CURVE
single curve or edge
|
static MatchedReferenceBuilder.Types |
CURVE_COLLECTOR
curve collector or edge collector
|
static MatchedReferenceBuilder.Types |
FACE
single face or datum plane
|
static MatchedReferenceBuilder.Types |
FACE_COLLECTOR
face collector
|
static MatchedReferenceBuilder.Types |
OBJECT
general geometry such as the target body and the tool body for copying unite feature
|
static MatchedReferenceBuilder.Types |
PLANE
plane
|
static MatchedReferenceBuilder.Types |
POINT
point
|
static MatchedReferenceBuilder.Types |
SECTION
section
|
static MatchedReferenceBuilder.Types |
UNDEFINED
default type for feature name lable
|
static MatchedReferenceBuilder.Types |
VECTOR
vector
|
Modifier and Type | Method and Description |
---|---|
static MatchedReferenceBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MatchedReferenceBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MatchedReferenceBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final MatchedReferenceBuilder.Types CURVE
public static final MatchedReferenceBuilder.Types FACE
public static final MatchedReferenceBuilder.Types CURVE_COLLECTOR
public static final MatchedReferenceBuilder.Types FACE_COLLECTOR
public static final MatchedReferenceBuilder.Types SECTION
public static final MatchedReferenceBuilder.Types POINT
public static final MatchedReferenceBuilder.Types VECTOR
public static final MatchedReferenceBuilder.Types OBJECT
public static final MatchedReferenceBuilder.Types BODY_COLLECTOR
public static final MatchedReferenceBuilder.Types CSYS
public static final MatchedReferenceBuilder.Types PLANE
public static final MatchedReferenceBuilder.Types AXIS
public static final MatchedReferenceBuilder.Types UNDEFINED
public static final int _CURVE
public static final int _FACE
public static final int _CURVE_COLLECTOR
public static final int _FACE_COLLECTOR
public static final int _SECTION
public static final int _POINT
public static final int _VECTOR
public static final int _OBJECT
public static final int _BODY_COLLECTOR
public static final int _CSYS
public static final int _PLANE
public static final int _AXIS
public static final int _UNDEFINED
public static MatchedReferenceBuilder.Types valueOf(int value)
public static MatchedReferenceBuilder.Types valueOf(String name)
public static MatchedReferenceBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.