public interface LinearDimensionBuilder extends DimensionBuilder
LinearDimension
builder
FeatureCollection.createLinearDimensionBuilder(nxopen.features.LinearDimension)
Property | Value |
---|---|
OrientationOption | OrientXpress |
Value.Value | 0 (millimeters part), 0 (inches part) |
Modifier and Type | Interface and Description |
---|---|
static class |
LinearDimensionBuilder.OrientationOptionType
the option that controls whether the OrientXpress or whether the vector block
Controls the orientation of the Linear Dimension
|
Modifier and Type | Method and Description |
---|---|
OrientXpressBuilder |
dimensionOrientation()
Returns the OrientXpress that is employed in the ADM Linear Dimension Feature
License requirements: None. |
nxopen.Direction |
dimensionOrientationVector()
Returns the dimension orientation vector for the Linear Dimension
License requirements: None. |
SelectNXObject |
measurementObject()
Returns the measurement object to which the ADM Linear Dimension is measured to
License requirements: None. |
LinearDimensionBuilder.OrientationOptionType |
orientationOption()
Returns the option that controls whether the OrientXpress or whether the vector block
Controls the orientation of the Linear Dimension
License requirements: None. |
SelectNXObject |
originObject()
Returns the origin object from which the ADM Linear dimension is measured from
License requirements: None. |
void |
setDimensionOrientationVector(nxopen.Direction dimensionOrientationVector)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
void |
setFaceToMove(Face face)
The important face that is being moved through the ADM Linear Dimension Feature.
|
void |
setOrientationOption(LinearDimensionBuilder.OrientationOptionType orientationOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
dimensionLocation, faceChangeOverflowBehavior, facesToMove, getDimension, saveConstraints, value
SelectNXObject originObject() throws NXException, RemoteException
NXException
RemoteException
SelectNXObject measurementObject() throws NXException, RemoteException
NXException
RemoteException
LinearDimensionBuilder.OrientationOptionType orientationOption() throws NXException, RemoteException
NXException
RemoteException
void setOrientationOption(LinearDimensionBuilder.OrientationOptionType orientationOption) throws NXException, RemoteException
orientationOption
- NXException
RemoteException
nxopen.Direction dimensionOrientationVector() throws NXException, RemoteException
NXException
RemoteException
void setDimensionOrientationVector(nxopen.Direction dimensionOrientationVector) throws NXException, RemoteException
dimensionOrientationVector
- NXException
RemoteException
OrientXpressBuilder dimensionOrientation() throws NXException, RemoteException
NXException
RemoteException
void setFaceToMove(Face face) throws NXException, RemoteException
face
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.