public static class LinearDimensionBuilder.OrientationOptionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ORIENT_XPRESS
Orientation option using Orient Xpress
|
static int |
_VECTOR
Orientation option using vector
|
static LinearDimensionBuilder.OrientationOptionType |
ORIENT_XPRESS
Orientation option using Orient Xpress
|
static LinearDimensionBuilder.OrientationOptionType |
VECTOR
Orientation option using vector
|
Modifier and Type | Method and Description |
---|---|
static LinearDimensionBuilder.OrientationOptionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LinearDimensionBuilder.OrientationOptionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LinearDimensionBuilder.OrientationOptionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final LinearDimensionBuilder.OrientationOptionType ORIENT_XPRESS
public static final LinearDimensionBuilder.OrientationOptionType VECTOR
public static final int _ORIENT_XPRESS
public static final int _VECTOR
public static LinearDimensionBuilder.OrientationOptionType valueOf(int value)
public static LinearDimensionBuilder.OrientationOptionType valueOf(String name)
public static LinearDimensionBuilder.OrientationOptionType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.