public static class LawExtensionBuilderEx.MiterOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BLEND
Creates a three-sided patch between two faces
|
static int |
_NONE
No miter solution between two discontinuous faces
|
static int |
_RADIUS
Creates a four-sided patch between two faces
|
static int |
_SHARP
Creates a sharp edge between two faces
|
static LawExtensionBuilderEx.MiterOptions |
BLEND
Creates a three-sided patch between two faces
|
static LawExtensionBuilderEx.MiterOptions |
NONE
No miter solution between two discontinuous faces
|
static LawExtensionBuilderEx.MiterOptions |
RADIUS
Creates a four-sided patch between two faces
|
static LawExtensionBuilderEx.MiterOptions |
SHARP
Creates a sharp edge between two faces
|
Modifier and Type | Method and Description |
---|---|
static LawExtensionBuilderEx.MiterOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LawExtensionBuilderEx.MiterOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LawExtensionBuilderEx.MiterOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final LawExtensionBuilderEx.MiterOptions NONE
public static final LawExtensionBuilderEx.MiterOptions SHARP
public static final LawExtensionBuilderEx.MiterOptions BLEND
public static final LawExtensionBuilderEx.MiterOptions RADIUS
public static final int _NONE
public static final int _SHARP
public static final int _BLEND
public static final int _RADIUS
public static LawExtensionBuilderEx.MiterOptions valueOf(int value)
public static LawExtensionBuilderEx.MiterOptions valueOf(String name)
public static LawExtensionBuilderEx.MiterOptions[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.