public static class GlobalShapingBuilder.PointMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_OFFSET_FROM_SHEET
Target point is offset from sheet
|
static int |
_POINT_DEFINED
Target point is the given point
|
static GlobalShapingBuilder.PointMethodType |
OFFSET_FROM_SHEET
Target point is offset from sheet
|
static GlobalShapingBuilder.PointMethodType |
POINT_DEFINED
Target point is the given point
|
Modifier and Type | Method and Description |
---|---|
static GlobalShapingBuilder.PointMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GlobalShapingBuilder.PointMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GlobalShapingBuilder.PointMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final GlobalShapingBuilder.PointMethodType OFFSET_FROM_SHEET
public static final GlobalShapingBuilder.PointMethodType POINT_DEFINED
public static final int _OFFSET_FROM_SHEET
public static final int _POINT_DEFINED
public static GlobalShapingBuilder.PointMethodType valueOf(int value)
public static GlobalShapingBuilder.PointMethodType valueOf(String name)
public static GlobalShapingBuilder.PointMethodType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.