public static class EmbossSidewall.SidewallMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CURVE_TAPERED
Indicates method to calculate tapered sidewall faces with reference to the taper direction.
|
static int |
_ISOCLINE_TAPERED
Indicates method to calculate tapered sidewall faces with reference to the taper direction and the taper reference curve tangents.
|
static int |
_NORMAL
Indicates method to calculate tapered sidewall faces with reference to the taper direction and the normal of the taper faces' original surfaces.
|
static int |
_OFFSET
(Not supported in NX4.)
|
static int |
_RULED
Indicates method to create sidewalls that are ruled along the normals of the faces in the supplied profile.
|
static int |
_SWEPT
Indicates method to create sidewalls that are swept.
|
static int |
_TWO_SECTION
(Not supported in NX4.)
|
static EmbossSidewall.SidewallMethod |
CURVE_TAPERED
Indicates method to calculate tapered sidewall faces with reference to the taper direction.
|
static EmbossSidewall.SidewallMethod |
ISOCLINE_TAPERED
Indicates method to calculate tapered sidewall faces with reference to the taper direction and the taper reference curve tangents.
|
static EmbossSidewall.SidewallMethod |
NORMAL
Indicates method to calculate tapered sidewall faces with reference to the taper direction and the normal of the taper faces' original surfaces.
|
static EmbossSidewall.SidewallMethod |
OFFSET
(Not supported in NX4.)
|
static EmbossSidewall.SidewallMethod |
RULED
Indicates method to create sidewalls that are ruled along the normals of the faces in the supplied profile.
|
static EmbossSidewall.SidewallMethod |
SWEPT
Indicates method to create sidewalls that are swept.
|
static EmbossSidewall.SidewallMethod |
TWO_SECTION
(Not supported in NX4.)
|
Modifier and Type | Method and Description |
---|---|
static EmbossSidewall.SidewallMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossSidewall.SidewallMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossSidewall.SidewallMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final EmbossSidewall.SidewallMethod ISOCLINE_TAPERED
public static final EmbossSidewall.SidewallMethod CURVE_TAPERED
public static final EmbossSidewall.SidewallMethod RULED
public static final EmbossSidewall.SidewallMethod SWEPT
public static final EmbossSidewall.SidewallMethod NORMAL
public static final EmbossSidewall.SidewallMethod TWO_SECTION
public static final EmbossSidewall.SidewallMethod OFFSET
public static final int _ISOCLINE_TAPERED
public static final int _CURVE_TAPERED
public static final int _RULED
public static final int _SWEPT
public static final int _NORMAL
public static final int _TWO_SECTION
public static final int _OFFSET
public static EmbossSidewall.SidewallMethod valueOf(int value)
public static EmbossSidewall.SidewallMethod valueOf(String name)
public static EmbossSidewall.SidewallMethod[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.