public static class DraftBuilder.Method extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ISOCLINE
Indicates use of isocline algorithm to create draft.
|
static int |
_TRUE_DRAFT
Indicates use of true draft algorithm to create draft.
|
static DraftBuilder.Method |
ISOCLINE
Indicates use of isocline algorithm to create draft.
|
static DraftBuilder.Method |
TRUE_DRAFT
Indicates use of true draft algorithm to create draft.
|
Modifier and Type | Method and Description |
---|---|
static DraftBuilder.Method |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBuilder.Method |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBuilder.Method[] |
values()
Returns an array that contains the values for this enum.
|
public static final DraftBuilder.Method ISOCLINE
public static final DraftBuilder.Method TRUE_DRAFT
public static final int _ISOCLINE
public static final int _TRUE_DRAFT
public static DraftBuilder.Method valueOf(int value)
public static DraftBuilder.Method valueOf(String name)
public static DraftBuilder.Method[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.