public static class DraftBodyBuilder.RepairingPartingEdgeOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
No repair parting edge option is specified
|
static int |
_WITH_FILLET
Repair concave miter corners with fillet
|
static int |
_WITH_LINE_AND_FILLET
Repair concave miter corners with both fillet and line
|
static DraftBodyBuilder.RepairingPartingEdgeOption |
NONE
No repair parting edge option is specified
|
static DraftBodyBuilder.RepairingPartingEdgeOption |
WITH_FILLET
Repair concave miter corners with fillet
|
static DraftBodyBuilder.RepairingPartingEdgeOption |
WITH_LINE_AND_FILLET
Repair concave miter corners with both fillet and line
|
Modifier and Type | Method and Description |
---|---|
static DraftBodyBuilder.RepairingPartingEdgeOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DraftBodyBuilder.RepairingPartingEdgeOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DraftBodyBuilder.RepairingPartingEdgeOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final DraftBodyBuilder.RepairingPartingEdgeOption NONE
public static final DraftBodyBuilder.RepairingPartingEdgeOption WITH_FILLET
public static final DraftBodyBuilder.RepairingPartingEdgeOption WITH_LINE_AND_FILLET
public static final int _NONE
public static final int _WITH_FILLET
public static final int _WITH_LINE_AND_FILLET
public static DraftBodyBuilder.RepairingPartingEdgeOption valueOf(int value)
public static DraftBodyBuilder.RepairingPartingEdgeOption valueOf(String name)
public static DraftBodyBuilder.RepairingPartingEdgeOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.