public interface DatumCsysBuilder
FeatureCollection.createDatumCsysBuilder(Feature)
Modifier and Type | Interface and Description |
---|---|
static class |
DatumCsysBuilder.WaveLinkInformationData
This class holds the data returned from
getWaveLinkInformation() |
Modifier and Type | Method and Description |
---|---|
boolean |
componentsCreation()
Deprecated.
Deprecated in NX7.5.1. This property is now always TRUE and calls to this property can be safely removed.
|
CartesianCoordinateSystem |
csys()
Returns the CSYS that defines a Datum CSYS
License requirements: None. |
double |
displayScaleFactor()
Returns the scale factor of the input Datum Csys
License requirements: None. |
boolean |
fixedSizeDatum()
Deprecated.
Deprecated in NX7.5.1. This property is now always TRUE and calls to this property can be safely removed.
|
DatumCsysBuilder.WaveLinkInformationData |
getWaveLinkInformation()
Prints wave browser type information about link
License requirements: wave ("WAVE FUNCTIONALITY") . |
void |
setComponentsCreation(boolean componentsCreation)
Deprecated.
Deprecated in NX7.5.1. This property is now always TRUE and calls to this property can be safely removed.
|
void |
setCsys(CartesianCoordinateSystem csys)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
void |
setDisplayScaleFactor(double displayScaleFactor)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
void |
setFixedSizeDatum(boolean fixedSizeDatum)
Deprecated.
Deprecated in NX7.5.1. This property is now always TRUE and calls to this property can be safely removed.
|
void setCsys(CartesianCoordinateSystem csys) throws NXException, RemoteException
csys
- exisiting WCS This parameter may not be null.NXException
RemoteException
CartesianCoordinateSystem csys() throws NXException, RemoteException
NXException
RemoteException
void setDisplayScaleFactor(double displayScaleFactor) throws NXException, RemoteException
displayScaleFactor
- display scale factorNXException
RemoteException
double displayScaleFactor() throws NXException, RemoteException
NXException
RemoteException
void setComponentsCreation(boolean componentsCreation) throws NXException, RemoteException
componentsCreation
- TRUE at creation and FALSE at edit
NXException
RemoteException
boolean componentsCreation() throws NXException, RemoteException
NXException
RemoteException
void setFixedSizeDatum(boolean fixedSizeDatum) throws NXException, RemoteException
fixedSizeDatum
- always TRUE at both of creation and edit
NXException
RemoteException
boolean fixedSizeDatum() throws NXException, RemoteException
NXException
RemoteException
DatumCsysBuilder.WaveLinkInformationData getWaveLinkInformation() throws NXException, RemoteException
NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.