public interface CutFaceBuilder
FeatureCollection.createCutFaceBuilder(Feature)
Property | Value |
---|---|
FaceToCut.CoaxialEnabled | 0 |
FaceToCut.CoplanarAxesEnabled | 0 |
FaceToCut.CoplanarEnabled | 0 |
FaceToCut.EqualDiameterEnabled | 0 |
FaceToCut.OffsetEnabled | 0 |
FaceToCut.ParallelEnabled | 0 |
FaceToCut.PerpendicularEnabled | 0 |
FaceToCut.SymmetricEnabled | 0 |
FaceToCut.TangentEnabled | 0 |
FaceToCut.ThicknessChainEnabled | 0 |
FaceToCut.UseFaceBrowse | 1 |
Motion.DeltaEnum | ReferenceWcsWorkPart |
Motion.DeltaXc.Value | 0.0 |
Motion.DeltaYc.Value | 0.0 |
Motion.DeltaZc.Value | 0.0 |
Motion.Option | DistanceAngle |
Modifier and Type | Method and Description |
---|---|
boolean |
doPaste()
Returns the do paste option defines whether paste the cut faces to a target body.
|
FaceRecognitionBuilder |
faceToCut()
Returns the face recognition builder holding the faces to cut.
|
ModlMotion |
motion()
Returns the motion about which the cut faces move
License requirements: None. |
boolean |
reverseDirection()
Returns the reverse direction.
|
void |
setDoPaste(boolean doPaste)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
void |
setReverseDirection(boolean reverseDirection)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
SelectBody |
targetBody()
Returns the target body.
|
FaceRecognitionBuilder faceToCut() throws NXException, RemoteException
NXException
RemoteException
ModlMotion motion() throws NXException, RemoteException
NXException
RemoteException
boolean doPaste() throws NXException, RemoteException
NXException
RemoteException
void setDoPaste(boolean doPaste) throws NXException, RemoteException
doPaste
- NXException
RemoteException
SelectBody targetBody() throws NXException, RemoteException
NXException
RemoteException
boolean reverseDirection() throws NXException, RemoteException
NXException
RemoteException
void setReverseDirection(boolean reverseDirection) throws NXException, RemoteException
reverseDirection
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.