public static class CopyPasteBuilder.ParentSelectOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_INPUT_FOR_ORIGINAL_PARENT
Specifying smart object using the same creation method that was used in the original feature.
|
static int |
_SMART_OBJECT
Selecting input for the original parent.
|
static CopyPasteBuilder.ParentSelectOption |
INPUT_FOR_ORIGINAL_PARENT
Specifying smart object using the same creation method that was used in the original feature.
|
static CopyPasteBuilder.ParentSelectOption |
SMART_OBJECT
Selecting input for the original parent.
|
Modifier and Type | Method and Description |
---|---|
static CopyPasteBuilder.ParentSelectOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CopyPasteBuilder.ParentSelectOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CopyPasteBuilder.ParentSelectOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final CopyPasteBuilder.ParentSelectOption SMART_OBJECT
public static final CopyPasteBuilder.ParentSelectOption INPUT_FOR_ORIGINAL_PARENT
public static final int _SMART_OBJECT
public static final int _INPUT_FOR_ORIGINAL_PARENT
public static CopyPasteBuilder.ParentSelectOption valueOf(int value)
public static CopyPasteBuilder.ParentSelectOption valueOf(String name)
public static CopyPasteBuilder.ParentSelectOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.