public static class CopyPasteBuilder.BuilderVersion extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXPOSE_BODY
Value of version which exposes additional target body parent; It should be added since NX8.5.
|
static int |
_EXPOSE_ONFLY_SO
Value of version which exposes smart object created on fly as part of the copy operation; It should be set since NX8.0.
|
static int |
_ORIGINAL
Value of original version; It can be set before NX8.0.
|
static int |
_SHOW_PARENT_SELECT_OPTION
Value of version which introduces parent select option; It should be added since NX8.5.1.
|
static CopyPasteBuilder.BuilderVersion |
EXPOSE_BODY
Value of version which exposes additional target body parent; It should be added since NX8.5.
|
static CopyPasteBuilder.BuilderVersion |
EXPOSE_ONFLY_SO
Value of version which exposes smart object created on fly as part of the copy operation; It should be set since NX8.0.
|
static CopyPasteBuilder.BuilderVersion |
ORIGINAL
Value of original version; It can be set before NX8.0.
|
static CopyPasteBuilder.BuilderVersion |
SHOW_PARENT_SELECT_OPTION
Value of version which introduces parent select option; It should be added since NX8.5.1.
|
Modifier and Type | Method and Description |
---|---|
static CopyPasteBuilder.BuilderVersion |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CopyPasteBuilder.BuilderVersion |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CopyPasteBuilder.BuilderVersion[] |
values()
Returns an array that contains the values for this enum.
|
public static final CopyPasteBuilder.BuilderVersion ORIGINAL
public static final CopyPasteBuilder.BuilderVersion EXPOSE_ONFLY_SO
public static final CopyPasteBuilder.BuilderVersion EXPOSE_BODY
public static final CopyPasteBuilder.BuilderVersion SHOW_PARENT_SELECT_OPTION
public static final int _ORIGINAL
public static final int _EXPOSE_ONFLY_SO
public static final int _EXPOSE_BODY
public static final int _SHOW_PARENT_SELECT_OPTION
public static CopyPasteBuilder.BuilderVersion valueOf(int value)
public static CopyPasteBuilder.BuilderVersion valueOf(String name)
public static CopyPasteBuilder.BuilderVersion[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.