public interface ChangeShellThicknessBuilder
ChangeShellThickness
builder FeatureCollection.createChangeShellThicknessBuilder(nxopen.features.ChangeShellThickness)
Property | Value |
---|---|
FacesToChangeThickness.CoaxialEnabled | 0 |
FacesToChangeThickness.CoplanarAxesEnabled | 0 |
FacesToChangeThickness.CoplanarEnabled | 0 |
FacesToChangeThickness.EqualDiameterEnabled | 0 |
FacesToChangeThickness.OffsetEnabled | 0 |
FacesToChangeThickness.ParallelEnabled | 0 |
FacesToChangeThickness.PerpendicularEnabled | 0 |
FacesToChangeThickness.SymmetricEnabled | 0 |
FacesToChangeThickness.TangentEnabled | 0 |
FacesToChangeThickness.ThicknessChainEnabled | 0 |
FacesToChangeThickness.UseFaceBrowse | 1 |
NeighborsEnabled | True |
WallThickness.Value | 5.0 (millimeters part), 0.5 (inches part) |
Modifier and Type | Method and Description |
---|---|
void |
addEntities(NXObject[] entities)
Adds entities which have same wall thickness value as the selected face
License requirements: None. |
FaceRecognitionBuilder |
facesToChangeThickness()
Returns the faces to be selected to change thickness
License requirements: None. |
boolean |
neighborsEnabled()
Returns the flag to select neighbor faces that have the same wall thickness value as the face selected.
|
void |
removeEntities(NXObject[] entities)
Removes entities
License requirements: None. |
void |
setNeighborsEnabled(boolean selectNeighbors)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Expression |
wallThickness()
Returns the wall thickness
License requirements: None. |
FaceRecognitionBuilder facesToChangeThickness() throws NXException, RemoteException
NXException
RemoteException
boolean neighborsEnabled() throws NXException, RemoteException
NXException
RemoteException
void setNeighborsEnabled(boolean selectNeighbors) throws NXException, RemoteException
selectNeighbors
- NXException
RemoteException
Expression wallThickness() throws NXException, RemoteException
NXException
RemoteException
void addEntities(NXObject[] entities) throws NXException, RemoteException
entities
- Objects to addNXException
RemoteException
void removeEntities(NXObject[] entities) throws NXException, RemoteException
entities
- Objects to removeNXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.