public static class BridgeCurveBuilder.CurveDirectionTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PERPENDICULAR
bridge direction takes the direction that is
perpendicular to the tangent direction
of the base curve at the selected point
|
static int |
_TANGENT
bridge direction takes the tangent direction
of the base curve at the selected point
|
static BridgeCurveBuilder.CurveDirectionTypes |
PERPENDICULAR
bridge direction takes the direction that is
perpendicular to the tangent direction
of the base curve at the selected point
|
static BridgeCurveBuilder.CurveDirectionTypes |
TANGENT
bridge direction takes the tangent direction
of the base curve at the selected point
|
Modifier and Type | Method and Description |
---|---|
static BridgeCurveBuilder.CurveDirectionTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.CurveDirectionTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.CurveDirectionTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeCurveBuilder.CurveDirectionTypes TANGENT
public static final BridgeCurveBuilder.CurveDirectionTypes PERPENDICULAR
public static final int _TANGENT
public static final int _PERPENDICULAR
public static BridgeCurveBuilder.CurveDirectionTypes valueOf(int value)
public static BridgeCurveBuilder.CurveDirectionTypes valueOf(String name)
public static BridgeCurveBuilder.CurveDirectionTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.