public static class AestheticFaceBlendBuilder.BlendType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CHORD_LENGTH
Chord Length will keep the appearance of a constant width blend through areas which have changing angles between the input walls.
|
static int |
_RADIUS
Radius of the rolling ball is used to create the tangent lines.
|
static AestheticFaceBlendBuilder.BlendType |
CHORD_LENGTH
Chord Length will keep the appearance of a constant width blend through areas which have changing angles between the input walls.
|
static AestheticFaceBlendBuilder.BlendType |
RADIUS
Radius of the rolling ball is used to create the tangent lines.
|
Modifier and Type | Method and Description |
---|---|
static AestheticFaceBlendBuilder.BlendType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.BlendType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.BlendType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AestheticFaceBlendBuilder.BlendType RADIUS
public static final AestheticFaceBlendBuilder.BlendType CHORD_LENGTH
public static final int _RADIUS
public static final int _CHORD_LENGTH
public static AestheticFaceBlendBuilder.BlendType valueOf(int value)
public static AestheticFaceBlendBuilder.BlendType valueOf(String name)
public static AestheticFaceBlendBuilder.BlendType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.