Package | Description |
---|---|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
Modifier and Type | Field and Description |
---|---|
static FeatureExtractionBuilder.InputActions |
FeatureExtractionBuilder.InputActions.BLANK
Blank the input facet bodies
|
static FeatureExtractionBuilder.InputActions |
FeatureExtractionBuilder.InputActions.DELETE
Delete the input facet bodies
|
static FeatureExtractionBuilder.InputActions |
FeatureExtractionBuilder.InputActions.RETAIN
Retain the input facet bodies
|
Modifier and Type | Method and Description |
---|---|
FeatureExtractionBuilder.InputActions |
FeatureExtractionBuilder.inputAction()
Returns the input facet body action
License requirements: None. |
static FeatureExtractionBuilder.InputActions |
FeatureExtractionBuilder.InputActions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FeatureExtractionBuilder.InputActions |
FeatureExtractionBuilder.InputActions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FeatureExtractionBuilder.InputActions[] |
FeatureExtractionBuilder.InputActions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FeatureExtractionBuilder.setInputAction(FeatureExtractionBuilder.InputActions inputAction)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.