Package | Description |
---|---|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
Modifier and Type | Field and Description |
---|---|
static DecimateFacetBodyBuilder.DecimateMethodType |
DecimateFacetBodyBuilder.DecimateMethodType.CHORDAL_DEVIATION
Chordal deviation reduces the number of facets by removing facets which do not effect the overall accuracy of the mesh.
|
static DecimateFacetBodyBuilder.DecimateMethodType |
DecimateFacetBodyBuilder.DecimateMethodType.PERCENTAGE
Percentage option allows the user to reduce the facet count by overall percentage.
|
static DecimateFacetBodyBuilder.DecimateMethodType |
DecimateFacetBodyBuilder.DecimateMethodType.SMALLEST_FACET
Smallest facet removes all facets smaller than the defined area, thus removing facets deemed to be redundant by the designer.
|
Modifier and Type | Method and Description |
---|---|
DecimateFacetBodyBuilder.DecimateMethodType |
DecimateFacetBodyBuilder.decimateMethod()
Returns the decimation method
License requirements: None. |
static DecimateFacetBodyBuilder.DecimateMethodType |
DecimateFacetBodyBuilder.DecimateMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DecimateFacetBodyBuilder.DecimateMethodType |
DecimateFacetBodyBuilder.DecimateMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DecimateFacetBodyBuilder.DecimateMethodType[] |
DecimateFacetBodyBuilder.DecimateMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DecimateFacetBodyBuilder.setDecimateMethod(DecimateFacetBodyBuilder.DecimateMethodType decimateMethod)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.