public static class BridgeFacetBodyBuilder.Input extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DELETE
Delete the input facet body after builder committing
|
static int |
_HIDE
Hide the input facet body after builder committing
|
static int |
_KEEP
Keep the input facet body after builder committing
|
static BridgeFacetBodyBuilder.Input |
DELETE
Delete the input facet body after builder committing
|
static BridgeFacetBodyBuilder.Input |
HIDE
Hide the input facet body after builder committing
|
static BridgeFacetBodyBuilder.Input |
KEEP
Keep the input facet body after builder committing
|
Modifier and Type | Method and Description |
---|---|
static BridgeFacetBodyBuilder.Input |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeFacetBodyBuilder.Input |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeFacetBodyBuilder.Input[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeFacetBodyBuilder.Input KEEP
public static final BridgeFacetBodyBuilder.Input DELETE
public static final BridgeFacetBodyBuilder.Input HIDE
public static final int _KEEP
public static final int _DELETE
public static final int _HIDE
public static BridgeFacetBodyBuilder.Input valueOf(int value)
public static BridgeFacetBodyBuilder.Input valueOf(String name)
public static BridgeFacetBodyBuilder.Input[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.