Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static ViewProjectionBuilder.CurveType |
ViewProjectionBuilder.CurveType.ACTIVE
Active
|
static ViewProjectionBuilder.CurveType |
ViewProjectionBuilder.CurveType.NONE
None
|
static ViewProjectionBuilder.CurveType |
ViewProjectionBuilder.CurveType.REFERENCE
Reference
|
Modifier and Type | Method and Description |
---|---|
ViewProjectionBuilder.CurveType |
ViewProjectionBuilder.curveTypeEdges()
Returns the curve type edges in the setting group
License requirements: None. |
ViewProjectionBuilder.CurveType |
ViewProjectionBuilder.curveTypePlane1()
Returns the curve type plane 1 in the setting group
License requirements: None. |
ViewProjectionBuilder.CurveType |
ViewProjectionBuilder.curveTypePlane2()
Returns the curve type plane 2 in the setting group , if the type is set to
one plane, the second plane information is ignored
License requirements: None. |
static ViewProjectionBuilder.CurveType |
ViewProjectionBuilder.CurveType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ViewProjectionBuilder.CurveType |
ViewProjectionBuilder.CurveType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ViewProjectionBuilder.CurveType[] |
ViewProjectionBuilder.CurveType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ViewProjectionBuilder.setCurveTypeEdges(ViewProjectionBuilder.CurveType type)
License requirements: nx_layout ("NX Layout") . |
void |
ViewProjectionBuilder.setCurveTypePlane1(ViewProjectionBuilder.CurveType type)
License requirements: nx_layout ("NX Layout") . |
void |
ViewProjectionBuilder.setCurveTypePlane2(ViewProjectionBuilder.CurveType type)
License requirements: nx_layout ("NX Layout") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.