Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Method and Description |
---|---|
ShipDraftingViewLinesBuilder |
DraftingViewCollection.createShipDraftingViewLinesBuilder()
Creates a
ShipDraftingViewLinesBuilder
License requirements: nx_ship_drafting ("Ship Drafting") Created in NX10.0.0 |
ShipDraftingViewLinesBuilder |
ShipDraftingViewLinesBuilderList.findItem(int index)
Returns the object at the input index.
|
ShipDraftingViewLinesBuilder[] |
ShipDraftingViewLinesBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ShipDraftingViewLinesBuilderList.append(ShipDraftingViewLinesBuilder object)
Appends an object to the list
License requirements: None. |
void |
ShipDraftingViewLinesBuilderList.append(ShipDraftingViewLinesBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ShipDraftingViewLinesBuilderList.erase(ShipDraftingViewLinesBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ShipDraftingViewLinesBuilderList.erase(ShipDraftingViewLinesBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ShipDraftingViewLinesBuilderList.findIndex(ShipDraftingViewLinesBuilder obj)
Finds the index where the input object appears.
|
void |
ShipDraftingViewLinesBuilderList.insert(int location,
ShipDraftingViewLinesBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ShipDraftingViewLinesBuilderList.setContents(ShipDraftingViewLinesBuilder[] objects)
Sets the contents of the entire list.
|
void |
ShipDraftingViewLinesBuilderList.swap(ShipDraftingViewLinesBuilder object1,
ShipDraftingViewLinesBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.