Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.StandardStyle.ANSI_STANDARD
Deprecated.
|
static SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.StandardStyle.ESKD_STANDARD
Deprecated.
|
static SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.StandardStyle.GB_STANDARD
Deprecated.
|
static SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.StandardStyle.ISO_STANDARD
Deprecated.
|
static SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.StandardStyle.ISO128STANDARD
Deprecated.
|
static SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.StandardStyle.JIS_STANDARD
Deprecated.
|
Modifier and Type | Method and Description |
---|---|
SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.standard()
Deprecated.
Deprecated in NX10.0.0. Use
ViewSectionLineBuilder.typeStandard() instead.
|
static SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.StandardStyle.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static SectionLineStyleBuilder.StandardStyle |
SectionLineStyleBuilder.StandardStyle.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static SectionLineStyleBuilder.StandardStyle[] |
SectionLineStyleBuilder.StandardStyle.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionLineStyleBuilder.setStandard(SectionLineStyleBuilder.StandardStyle standard)
Deprecated.
Deprecated in NX10.0.0. Use
ViewSectionLineBuilder.setTypeStandard(nxopen.drawings.ViewSectionLineBuilder.DisplayType) instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.