Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static GeneralWorkFlowBuilder.SettingsOrientationType |
GeneralWorkFlowBuilder.SettingsOrientationType.DRAWING_STANDARD |
static GeneralWorkFlowBuilder.SettingsOrientationType |
GeneralWorkFlowBuilder.SettingsOrientationType.DRAWING_TEMPLATE |
Modifier and Type | Method and Description |
---|---|
GeneralWorkFlowBuilder.SettingsOrientationType |
GeneralWorkFlowBuilder.settingsOrigination()
Returns the option that indicates the settings origination
License requirements: None. |
static GeneralWorkFlowBuilder.SettingsOrientationType |
GeneralWorkFlowBuilder.SettingsOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeneralWorkFlowBuilder.SettingsOrientationType |
GeneralWorkFlowBuilder.SettingsOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeneralWorkFlowBuilder.SettingsOrientationType[] |
GeneralWorkFlowBuilder.SettingsOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeneralWorkFlowBuilder.setSettingsOrigination(GeneralWorkFlowBuilder.SettingsOrientationType settingsOrigination)
License requirements: drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.