Package | Description |
---|---|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
Modifier and Type | Field and Description |
---|---|
static AddRemoveBoxViewBuilder.ModeType |
AddRemoveBoxViewBuilder.ModeType.ADD
Add mode
|
static AddRemoveBoxViewBuilder.ModeType |
AddRemoveBoxViewBuilder.ModeType.REMOVE
Remove mode
|
Modifier and Type | Method and Description |
---|---|
AddRemoveBoxViewBuilder.ModeType |
AddRemoveBoxViewBuilder.mode()
Returns the mode type
License requirements: None. |
static AddRemoveBoxViewBuilder.ModeType |
AddRemoveBoxViewBuilder.ModeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AddRemoveBoxViewBuilder.ModeType |
AddRemoveBoxViewBuilder.ModeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AddRemoveBoxViewBuilder.ModeType[] |
AddRemoveBoxViewBuilder.ModeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AddRemoveBoxViewBuilder.setMode(AddRemoveBoxViewBuilder.ModeType mode)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.