Package | Description |
---|---|
nxopen.drafting |
Provides classes and interfaces for the Drafting.
|
Modifier and Type | Method and Description |
---|---|
AttributeItemBuilder |
AutomationManager.createAttributeItemBuilder()
Creates a
AttributeItemBuilder
License requirements: None. |
AttributeItemBuilder |
AttributeItemBuilderList.findItem(int index)
Returns the object at the input index.
|
AttributeItemBuilder[] |
AttributeItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
AttributeItemBuilderList.append(AttributeItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
AttributeItemBuilderList.append(AttributeItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
AttributeItemBuilderList.erase(AttributeItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
AttributeItemBuilderList.erase(AttributeItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
AttributeItemBuilderList.findIndex(AttributeItemBuilder obj)
Finds the index where the input object appears.
|
void |
AttributeItemBuilderList.insert(int location,
AttributeItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
AttributeItemBuilderList.setContents(AttributeItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
AttributeItemBuilderList.swap(AttributeItemBuilder object1,
AttributeItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.